DOUT#.SOURCEID

Description

DOUT#.SOURCEID sets the digital output source ID, for sources that require an ID.

Examples

Usage

DOUT#.SOURCEID can be used to select the compare channel when DOUT#.SOURCE = 4 (Compare).

Code

The following commands set the source of digital output 2 to compare channel 1, and digital output 3 to compare channel 2.

--> DOUT2.SOURCE 4
--> DOUT2.SOURCEID 1
--> DOUT3.SOURCE 4
--> DOUT3.SOURCEID 2

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000  
Added Compare channel support 02-06-00-000  

General Information

Type Read/Write
Units N/A
Range 1 to 2
Default Value 0
Data Type Integer
See Also N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DOUT1.SOURCEID

360ah

02h

Unsigned8

-

-

Read/Write

No

DOUT2.SOURCEID

360bh

02h

Unsigned8

-

-

Read/Write

No

DOUT3.SOURCEID

360ch

02h

Unsigned8

-

-

Read/Write

No

DOUT4.SOURCEID

360dh

02h

Unsigned8

-

-

Read/Write

No

DOUT5.SOURCEID

360eh

02h

Unsigned8

-

-

Read/Write

No

DOUT6.SOURCEID

360fh

02h

Unsigned8

-

-

Read/Write

No

DOUT7.SOURCEID

3610h

02h

Unsigned8

-

-

Read/Write

No

DOUT8.SOURCEID

3611h

02h

Unsigned8

-

-

Read/Write

No

DOUT9.SOURCEID

3612h

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

DOUT1.SOURCEID

21200

52D0

Unsigned8

Read/Write

-

DOUT2.SOURCEID

21201

52D1

Unsigned8

Read/Write

-

DOUT3.SOURCEID

21202

52D2

Unsigned8

Read/Write

-

DOUT4.SOURCEID

21203

52D3

Unsigned8

Read/Write

-

DOUT5.SOURCEID

21204

52D4

Unsigned8

Read/Write

-

DOUT6.SOURCEID

21205

52D5

Unsigned8

Read/Write

-

DOUT7.SOURCEID

21206

52D6

Unsigned8

Read/Write

-

DOUT8.SOURCEID

21207

52D7

Unsigned8

Read/Write

-

DOUT9.SOURCEID

21208

52D8

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

DOUT1.SOURCEID

21200

Unsigned8

Read/Write

-

DOUT2.SOURCEID

21201

Unsigned8

Read/Write

-

DOUT3.SOURCEID

21202

Unsigned8

Read/Write

-

DOUT4.SOURCEID

21203

Unsigned8

Read/Write

-

DOUT5.SOURCEID

21204

Unsigned8

Read/Write

-

DOUT6.SOURCEID

21205

Unsigned8

Read/Write

-

DOUT7.SOURCEID

21206

Unsigned8

Read/Write

-

DOUT8.SOURCEID

21207

Unsigned8

Read/Write

-

DOUT9.SOURCEID

21208

Unsigned8

Read/Write

-